This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ51052B: replacement for max20356

Part Number: BQ51052B
Other Parts Discussed in Thread: BQ51050B, BQ25180

Hi Team,

I am looking for a replacement of max20356.

The applications is power solution for LED OHR (very fast transient responses are needed).

The cross reference tool suggests BQ51052B but I am not sure if this is the best solution.
What would you recommend here?

BR,
Stefan

  • Hi Stefan

    The BQ51050B is a wireless power battery charger will not be a good fit.

    The max20356 looks more like a the BQ25180 / 181.

    But MAX20356 is a large device with a lot of features and will not have a single IC solution.