The application is using TLVH431 and LP2951’s in avionics. The spec sheets for these parts have a storage temp range -65C to 150C but a recommended operating temp range of -40 to 125C. We need to understand the behavior of the devices in the -55 to -40C range. Is it just a tolerance or current handling issue? We see some plots down to -50C for various parameters. We are trying to establish the behavior so we will not need to test every device. In our application, these devices are significantly derated from your specs and they are non-precision applications; the temperature typically wouldn’t be in that unspecified band but we need to understand behavior there for startup and to insure there are no anomalies such as oscillations.
Thanks,
Eric