I designed a custom pcb using Beaglebone black designs and pmic's datasheets. I powered the pmic from the AC and USB pins, and when there is a fluctuation in input power or if the power goes off for 1-2 seconds, the pmic crashes, but if the power goes on and off for more than 10 seconds, it works normally without locking up. When I press the PB_IN button, pmic returns to normal. How can I get it back to normal without pressing the PB_IN button? How can I prevent Pmic crashing?