Part Number: LM5146
Other Parts Discussed in Thread: LM5141
hi team,
my customer is using LM5146 and they want to use it at heavy load and they want to avoid over current protection at application.
If I can relax the protective detection window to 4 ~ 10ms so that can support the system work, also can do DC short circuit protection
Can I add low pass to this detection window by using this capacitance in the manual diagram? The main concern is that the addition of a large capacitance in this place affects the setting of the overcurrent protection reference,
Because LM5146 has an over current protection trigger cycle of 128 cycles The current switch frequency we configure is about 500khz which makes the protection detection window much less than 1ms