This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61200 - Operating two devices in parallel, what is the leakage current for the device that is disabled?

Other Parts Discussed in Thread: TPS61200

I have an application where two TPS61200 devices have their Vout pins connected together. Both devices are set to produce the same output voltage but only one device is enabled at a time (each device has a different power source). Is this type of configuration allowed with the TPS61200? What is the leakage current for the device that is disabled when the other one is enabled?

Can Crhis Glaser please respond to this message, he has responded to other TPS61200 style questions.

Best Regards,

-David