Other Parts Discussed in Thread: TLC6C598-Q1
Hello team,
is it possible without SW adoptions to change a combination of 74HC595 + ULN2803 by the TPIC6C595?
The loads are small signal relays with ~10ma current per channel.
Questions 1: Is TPIC6C595 completely identical from a SW point of view?
Question 2: What is the max clock frequency for SRCK for RT and temp range -40°...+85°C
Thanks and best regards,
Michael