Hello experts,
I'd like to confirm which JEDEC environment and JEDEC thermal board are used for each thermal metric in LMR38020. I drew the table below.
Could you check wthether my understanding is correct?
Thermal Metric | Measurement Environment | Board uesd for a measurement |
ThetaJA | JESD51-2A | JESD51-7 High-k board with vias defined in JESD51-5 |
ThetaJA(Effective) | JESD51-2A | LMR38020 EVM board |
ThetaJC(top) | JESD51-14 | No board. Dierct connection with a heat sink or thermal grease is used between a DUT and a heat sink. |
ThetaJB | JESD51-8 | JESD51-7 High-k board |
PsiJT | JESD51-2A | JESD51-7 High-k board with vias defined in JESD51-5 |
PsiJB | JESD51-2A | JESD51-7 High-k board with vias defined in JESD51-5 |
ThetaJC(bot) | JESD51-14 | No board. Dierct connection with a heat sink or thermal grease is used between a DUT and a heat sink. |
Regards,
Kento