This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS562200: Regarding the parameter calculation of RC Snubber circuit, I have seen different descriptions in TI application manual. Would you like to confirm which is more reasonable?

Part Number: TPS562200

Regarding the parameter calculation of Snubber circuit, I have the following questions, please help to point out:

The first question: I have seen different descriptions of Rsnb values in different application manuals of TI. Would you like to confirm which is more reasonable? What is the value logic?

① In the application manual of TI -ZHCAA52, Chapter 3 Snubber buffer circuit mentioned Rsnb=√Lp/Cp (Lp is parasitic inductance, Cp is parasitic capacitance);

② It is mentioned in the Snubber parameter calculation in Section 1.3 of the TI application manual -ZHCA658 that R≥0.5x√Lp/Cp;

In addition, in Rohm's application manual "Snubber Circuit for Buck Converter IC", it is found that the Snubber parameter calculation is R=0.65x√Lp/Cp;

The second question: Regarding the value of Csnb, I have the following questions:

① Equation 11 in the TI application manual -ZHCA658 mentions that 1/2πf1Csnb=R/4, do not understand how this formula is obtained?

② It is mentioned in the application manual of TI -ZHCAA52 that Csnb=Cadd=3xCp, and I also saw in the application manual of Rohm that the value of Cp is 1-4 times. What is the logic here?

The above problems, have consulted a number of technical documents, most of them only write the result, did not mention the process logic, please also help to point under, thank you!

Related documents:

https://fscdn.rohm.com/en/products/databook/applinote/ic/power/switching_regulator/buck_snubber_app-e.pdf

https://www.ti.com.cn/cn/lit/an/zhcaa52/zhcaa52.pdf?ts=1711639516210&ref_url=https%253A%252F%252Fcn.bing.com%252F&_ticdt=MTcxMzE5MzkzMXwwMTdkMjQwYzI0M2EwMDExNWY0NDY2ZTg0M2EzMDUwNzIwMDE2MDZhMDA3ZTh8R0ExLjIuMTk4MDMxMTcyMi4xNjM2OTg3MzE3fG51bGx8bnVsbHxHUzEuMS4xNzEzMTkxNjQ4LjIyLjEuMTcxMzE5MzkzMS4wLjAuMHxudWxsfG51bGx8bnVsbA

https://www.ti.com/cn/lit/an/zhca658/zhca658.pdf?ts=1710544725645