Other Parts Discussed in Thread: BQ25756EVM, TPS25751, BQ25756
Hello,
I'm having some issues getting started with BQ25756EVM with TPS25751EVM.
So i'm going step by step
1. I tested TPS25751 alone, all good, source and sink.
2, Now wanted to test only sourcing at 5V from BQ charger.
I used the default configuration that allows sink and source from BQ and source 5V from PP5V but in the advanced settings, i changed the 5V source PDO to PP3 source this PDO (i understand this is to supply 5V PDO from PPHV?)
The result, it seems when i connect a USB key to J3, both PPHV and PP5V will close and TPS25751 will detect reverse current since PPHV (3.4V) is lower than PP5V (5.5V) or another error is detected USB is powered only 125ms and will reset non-stop.
Also, i'm powering Vsys of TPS25751 from Vbat of BQ25756 (8V) and in this configuration, i am not able to flash the 25751, i always need to change J1 jumpers to power from USB J2 to flash. Same issue with Vbat = 15V.