This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM74670-Q1: Looking for an alternative to the LM74670-Q1 which can handle higher frequency.

Part Number: LM74670-Q1

Is anyone aware of a "zero IQ" rectifier which can rectify up to 3kHz?

I'm working on a project that needs to rectify the 3-phase output from a wind-turbine; it produces up to 3kHz. This will be used for a power application as well; my main goal is to avoid heat losses when using a traditional 3 phase diode bridge rectifier.