This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS55289: crossover frequency

Part Number: TPS55289

hi team:

We recently tested the frequency response of TPS552892QWRYQRQ1 circuit attached, the results shows phase margin (61.7°) and gain margin(13.6db) pass the criteria, but crossover frequency is lower than 10kHz, which means the bandwidth of this circuit is lower than 10kHz. And we found most of buck-boost has low crossover frequency.

My question is:

1. Is low bandwidth (lower than 10kHz) of regulator acceptable if load transient meets requirement?

2. Do buck-boost and boost have lower bandwidth than buck in general? if yes, why?

3. I can adjust crossover frequency by optimizing compensation network, but the optimized bandwidth should be limitied by the regulator itself no matter how I change the comp network, so how do I know the bandwidth limitation of the regulator?

Thanks.