This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92662A-Q1: SYNC configuration

Part Number: TPS92662A-Q1


Hello team,

Hope you are doing well.

There are 14 pcs TPS92662A-Q1 in 8 PCB board in customers design, all devices need to be synced, there are HW and SW Synchronization.

1. For Hardware Synchronization, all devices must be clocked by the same clock, so how to deal with 92662A in different PCB, is it necessary to connect with separated wire for SYNC signal between different boards? And what is the influence?  Will the clock signal be affected by EMI?

2. For Software Synchronization, from customers experience, they SYNC 3 pcs by SW method, but they are not sure if it is available for 14pcs 92662A? So is there any recommendations or points to focus on?

Thanks!