Hi Team,
Could you please help check and confirm if TPS22992 can work normally when Vin is slightly >Vbias? that is Vbias=3.3V and Vin=3.6V.
Thanks.
Regards,
Nandan S M
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hey Nandan,
Having Vin>Vbias is not in the recommended operation conditions. The recommended operation conditions are below:
If this condition is really needed, it can be done at a short amount of time.
I still would suggest to connect Vbias pin to Vin if possible which would solve your issue.
Thanks,
Sam