Other Parts Discussed in Thread: TPS922055, TPS922054
Hello, I have a question.
I'm currently trying to turn on a 12V LED using a Li-ion battery with 3 series.
Conditions to be used
1. Vin = 8V~12.6V
2. Vled = 12V
3. Iled = 2.5A
4. PWM dimming
- The key question is whether the buck boost of the TPS923655 allows the LED to be controlled without any problems when changing the input voltage including the LED's Vf.
- In addition, I would like to inquire whether there is a substitute available under the above conditions.
Thanks