The chip used for UC1843MKGD1 is named SMGNAC1843PS.
The chip used for UC1843TD1/2 and UC1843-W is named SMGNC1843PS.
What is the difference of the chips? are they tested and released as the same ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The chip used for UC1843MKGD1 is named SMGNAC1843PS.
The chip used for UC1843TD1/2 and UC1843-W is named SMGNC1843PS.
What is the difference of the chips? are they tested and released as the same ?
Hey Joanne,
Which orderable part number did you use when ordering the die?


There is an A version and a non-A version of the die to order from.
The differences are largely current draw and different tolerances as one was an update of the other one.
Thanks,
Daniel