Other Parts Discussed in Thread: LM5156, LM51561
Hi,
I am designing a flyback converter 75W with a hiccup function for mass production.
The hiccup happens continuously, but the current limit is not reached(verified transformer current and voltage on CS pin < 100mV).
2.5V on the UVLO, frequency is 180 kHz.
If I use LM5156 without hiccup, the design works fine and reaches full power.
What could trigger hiccup besides current?
Please help.