Other Parts Discussed in Thread: TPSM8287A06, TPSM82866A, TPSM8287A12, TPSM8287A10
Hello,
I have three question in blue below.
Design requirements:
- Vin = 5 V
- Vout = 3.3 V
- I_LOAD max < 6 A
- C_LOAD = large and application dependent.
- Application in question: About 370 uF of nominal capacitance from ceramic capacitors distributed on the motherboard (where the TPSM82816 3.3 V regulator is placed) + 800 uF of tantalum capacitors on a daughter board (PMC module) connected to the motherboard through multiple board-to-board connectors.
- The 370 uF on the motherboard is fixed.
- The 800 uF on the daughter board could be much less depending on the third-party daughter board model. 800 uF (from tantalum capacitors) is currently the maximum value encountered. 10 uF (from tantalum capacitors) is currently the minimum value encountered.
- Application in question: About 370 uF of nominal capacitance from ceramic capacitors distributed on the motherboard (where the TPSM82816 3.3 V regulator is placed) + 800 uF of tantalum capacitors on a daughter board (PMC module) connected to the motherboard through multiple board-to-board connectors.
From the TPSM82816 data sheet:
- The recommended maximum effective output capacitance is 470 uF.
- Section 8.3.3: "The minimum output capacitance in Table 8-1 is for capacitors close to the output of the device. If the capacitance is distributed, a lower compensation setting can be required."
- What is considered "close to the output of the device?"
- Can additional capacitance beyond 470 uF be present if it is far enough, like on the daughter board in the example in the design requirements above?
- R1, R2, and C_FF values in table 9-2 (88.7k. 19.6k, and 3 pF, respectively) are different from the online Webench values (453k, 100k, and 0.59 pF, respectively). Both sets meet the data sheet requirements. High efficiency at loads below 0.1 A is not required. The device mode is set to PSM.
- Is one set of values better than the other?
If TPSM82816 is not suitable because of C_LOAD, please suggest an alternative that meets the given design requirements.
Thank you.