Hello guys,
Two of my customers use UCC27424 for their mass-production.
The device datasheet was changed recently.
At this moment, they have the following questions about the datasheet.
Could you please give me your reply?
Q1.
The following are deferent points of output resistance between UCC27424 new and old datasheet.
Datasheet Version : SLUS545E(OLD) SLUS545F(New)
Output resistance high(ohm) : Min/Typ/Max --> 18/--/45 Min/Typ/Max --> --/1.2/2.5
Output resistance low(ohm) : Min/Typ/Max --> 1.2/--/4.0 Min/Typ/Max --> --/0.7/1.2
Output resistances of UCC27424 new chip are improved very much from old chip.
Is measurement method and condition of the output resistance same in new chip and old chip?
Q2.
If Q1 answer is yes, what is the cause of this improvement?
Is it the switch elements (PMOS, NMOS, Bipolar NPN transistor) drivability improvement at new process?
Or the switch element size was changed bigger to be reduced output resistances?
Q3.
Why didn't TI design the output resistance value to be the similar with the old chip?
Your reply would be much appreciated.
Best regards,
Kazuya.