Other Parts Discussed in Thread: BQSTUDIO, , EV2400
Hello,
I'm having a failure "A read of data written failed comparison" when enabling VEN_EN bit or changing the flash update ok voltage.
I'm using a 4S Lifepo4, own circuit with BQ34110 and EV2400, bqstudio 1.3.124.
Im using a voltage divider network in my circuit with 250k and 16.5k ohms.
The problem seems to be that the voltage reading is only 3mV. what may i have missed?