Hi Experts,
Is it acceptable to use the TPS2121 under the following conditions?
When there is no power supplied to IN1 or IN2, an independent 3.3V is provided to PR1. During power-down, the 3.3V to PR1 is dropped after IN1 and IN2 have been turned off. The Recommended Operating Conditions in the datasheet state that PR1 can range from 0V to 5.5V, and there are no specific instructions regarding the sequence.
However, if there are any recommendations such as it being better to supply PR1 through a voltage divider from IN1, please let me know.
Best Regards.