Other Parts Discussed in Thread: BQ25622, BQ25620
Datasheet section 8.3.10.3.1 states that
When the BQ25628 is in OTG mode, Q1 is off to block power from PMID to VBUS.
in section 8.6.2.9, REG0x14 bit 7 'Q1_FULLON' is described as
Forces RBFET (Q1) into low resistance state (26 mΩ) , regardless of IINDPM setting. 0h = RBFET RDSON determined by IINDPM setting (default) 1h = RBFET RDSON is always 26 mΩ
can Q1 be forced into the low resistance state doring OTG operation, effectively allowing power to be sourced via the VBUS pin (instead of PMID)?