Hello TI,
In the datasheet, it describes that:
"The current through the internal PP_5V path are current limited to I LIM5V. The I LIM5V value is configured by application firmware."
1) Where can this be configured? Changing the PDO does not change the limiter or the Rp value.
Also the manual describes:
In section "PP_5V Power Switch Characteristics" 4 modes are described (+1 without a number).
2) Where can these modes be selected.
Thanks,
/Peter, GN Great Nordic.