This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problem in configuring the UCD9222 + UCD7242

Other Parts Discussed in Thread: UCD7242, UCD9222, TMS320C6678

Hi

I download the .xml file that is used in TMS320C6678 EVM.I make a PCB with UCD9222 and UCD7242 on it. After I import the project file that i download into Fusion Digital Power Designer(online Mode),I can connect the chip of UCD9222,and i can see the real-time information of the project displayed in  Monitor Task.Input level of UCD9222 is 12V,and Vin window displays correctly.But Vout rail displays that output level is 1.6V.All of two rails are 1.6V.The duty cycle is %0.0.It seems like the UCD9222 is disabled.I test the output level in board and the output level is 0V.I create a new project files but the result is the same.Do I make a mistake in configuring the chip?Why the PWM duty circle is %0 and Out level is always 1.6V displayed in monitor task?