This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC2805-Q1: UCC2805-Q1, UCC2803-Q1

Part Number: UCC2805-Q1


hello? My name is HL mando researcher Seongtaek Oh. 

Currently, we are using UCC2805-Q1 as a Flyback SMPS power device in our internal project.

Here, the output of the SMPS (= used as gate driver power) requires more load. As a result of taking the duty, I estimate that about 60% to 70% is needed.

However, the UCC2805 device showed a drop in output voltage when it exceeded 50% Max (=this can be confirmed in the datasheet).

We would like to replace it with the UCC2803-Q1 device, which increases the Duty Cycle Max to 100%.

As a result of checking the datasheet, it is determined that only the Duty Cycle Max value increases and the other specifications are completely the same for the two devices.

Please review whether there will be any issues when replacing only the IC element in the same circuit from UCC2805 to UCC2803.