This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPSM63606: My design is not operating when I turn on power

Part Number: TPSM63606


Hi TI Expert,

I am using TPSM63606 in design, step down my Vin (12/24V) to 5V,6A for other buck converter on board.

So I just copying the application circuit datasheet p.22 and layout on p.32,

but when I turn on power (12V), I see EN pin voltage up to 1.67V, but I see no output on VCC / Vout

Is there something i missed in my circuit?

Thanks and Best Regards,

Alex.

Attaching Sch and probed output waveform