Part Number: LM5025AEVAL
Hi,
I built a circuit using the LM5025AEVAL, but the output voltage is only 1.3V, and the transformer makes a strange noise. What could be the possible reasons for these issues?
Thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LM5025AEVAL
Hi,
I built a circuit using the LM5025AEVAL, but the output voltage is only 1.3V, and the transformer makes a strange noise. What could be the possible reasons for these issues?
Thank you.
Hi,
If that is the circuit you followed exactly, then you can measure each waveform to compare between yours and the EVM to trace where you see difference, starting with switching frequency, gate drive, Vds, etc.
Since you followed that circuit, then no need to review as the EVM works just fine. Your circuit does not work then there has to be something you did not build correctly you need to compare one circuit at a time to trace all then you can find where you got something wrong, then fix that, your board will work like the EVM.
Hi,
What was the input voltage and the load current?
In this below, both OUTA and OUTB off. You need to find what caused both of them off. VCC, CS1, SS, COMP, etc. Capture each of these along with OUTA and OUTB off and on to see any of them not in the correct range, or trigger protection.

Hi,
It looks CS2 threshold was triggered as soft start present.
Note CS2 (and CS1) threshold is only 0.25V. The waveform shows CS1 much higher than 0.25V. You need to reduce the current sense noise to resolve this issue as first step.