This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7H2201-SP: AVG SPICE model for AC analysis

Part Number: TPS7H2201-SP

Hello,

I was wondering if you had an AVG SPICE model for the TPS7H2201-SP. If so, could you post that on the device page?

Thank you,

Zackery Painter

  • Hi Zackery,

    We do not have an average model for the TPS7H2201-SP. Can you let me know the reason you are asking for one?

    Average models are used for AC analysis of switching converters in SPICE programs. As a load switch, the TPS7H2201-SP should only switch on or off when an event triggers it and not continuously during normal operation - hence it does not need to be averaged. We do offer a transient model to simulate with for those purposes.

    Thanks,

    Sarah