Other Parts Discussed in Thread: BQSTUDIO, EV2400,
Hi,
Having conducted several tests with the BQ35100EVM, I encountered an issue wherein the EOS bit doesn't change as expected.
Despite applying the prescribed pulse, the voltage fails to 0V.
Here is the setup I made :
So I use a primary cell and try to activate the EOS flag.
Here is the pulse I made :
To observe the EOS bit change, I have been aging the battery by imposing a load to discharge at 132 mA for 6 hours per day. I also allow the battery to rest for 16 hours to fully relax.
I conduct one test per day, but the EOS doesn't change.
Would it be possible to have some help in triggering the EOS bit ?
Best regards.