Dear Sir Madam
I am trying to figure out if UCD3138 is a good fit for my application or not. I need a 1MHz PWM signal where frequency is fixed and duty cycle is directly controlled by external analog signal. Is it possible to bypass the PID controller and have 1). Set the DPWM period register to a fixed value. 2) Set the event registers (DPWMEV1:4) and eventually duty cycle directly from digitized Error ADC (while bypassing the compensator loop).
In other word, the analog signal that we feed to EAP and EAN directly set the duty cycle without affecting the period.
I guess I couldn't find a way to do that because : 1) The input for DPWM should come from compensator and should pass through the PID loop and 2) The 24 bit output of compensator is split into two 14 bits one for duty cycle and other for period and there is no way to keep the period unaffected.
Also, is there other high resolution PWM generator that fits better to my project requirement?
Thanks
Kaveh