Other Parts Discussed in Thread: TPS7A24
Say I have the LP2981-50DBVR, the 5V part. Can I bias up the GND pin (say use a Schottky with 0.5V Vf between it and GND) and make it 5.5V? Will the performance be degraded?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Thank you for your question.
Please allow me 2-3 business days to reply to your question.
Best Regards,
Hannah
Just to clarify, are you asking if you can use a Schottky diode between OUT and GND?
Yes. Schottky (with a resistor, like 20K or so, to provide extra current from Vin to the diode's A; the diode, again, is between the GND pin and the GND)
Thank you for the clarification. Please allow me a couple business days to clarify with peers.
Best Regards,
Hannah
I believe the voltage on the GND pin is allowed to move in the circuit. I believe any noise at the GND pin would show up in the output voltage, because the reference is moving. As a result, the noise shouldn't be any lower than Vin noise except from what you are filtering out. If noise is mandatory for your application, we do not recommend moving forward with this design. If too much current tries to enter the GND pin, but your voltage exceeds the threshold voltage on the diodes, then this design should reroute the excess current through the diodes. In turn, this could save the part from damage. If you are intending for the GND pin to be RC filtered, you may be able to put the filter on the input instead.
I think a voltage divider with a potentiometer on the GND pin may be easier to set the output voltage to your desired output. This is not a standard way of how we use our LDOs, but these are my thoughts on the matter.
The TPS7A24 device is a pin for pin device with the same functionality as the LP2981: TPS7A24 data sheet, product information and support | TI.com
This device also has a FB resistor network, which allows for an adjustable output. This device would allow you to meet the 5.5V requirement for your project.
Best Regards,
Hannah