Hello,

Best Regards,
Hiroyuki Taguchi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Best Regards,
Hiroyuki Taguchi
Hi,
I would like to ask an additional question.
Q1.
In the case of VIN1=floating, VIN2=USB VBUS 5V input, 5V is output to VOUT, but is it correct to understand that it is operating in the mode shown in the red frame in the figure below?
Q2.
Which input, VIN1 or VIN2, is used for the power supply of "Control logic and gate drivers" in the datasheet Function Block Diagram?
Best Regards,
Hiroyuki
Hi Hiroyuki-san,
It looks like your part has been damaged. I see only 1uF capacitance on the inputs - I've seen before where when the part switches over, cable inductance and switched power supply delay cause the input voltage to temporarily go over 6V and that breaks the part. Can you swap the part with a new one and confirm the behavior, and if that's the case, put a bigger input capacitance on the device?
Q1. Yes, that's correct.
Q2. Whichever input is higher powers the device circuitry - there's a description of this in the Iq section of the data sheet Electrical Characteristics table.
Thanks,
Patrick
Hi Patrick,
Thank you for your reply.
I will replace the device with a normal one and check if it temporarily exceeds 6V.
I understand the answers to Q1 and Q2. thank you.
Thanks,
Hiroyuki
Hi Hiroyuki-san,
Thank you, please let me know the results and if you have additional questions.
Thanks,
Patrick