Hello
We are reviewing our designs to consider outcomes from single BMS board failures. We can evaluate and test many protections by shorting (in analysis and actual testing) either the discharge FET (during discharge) or charge FET during charging. If the FET cannot turn off, the CUV, COV, or over-temperature PF protections will trigger.
The battery sense inputs open-wire detection allows the PF to trigger for cell voltage sensing loss.
But if one of the series resistors between the current shunt and SRP or SRN pins develops a dry joint, is there internal "open-wire" like sensing for these pins for the BQ to respond to this failure ?
I haven't been able to find a protection status and event in the registers to show this so we want to work though safety when pack current and short circuits cannot be detected.
I am arranging to access the functional safety documents but I thought this might be useful as a forum question.
All the best
Harry