The numerical value does not appear in the Electrical Characteristics table in Section 7.5. Please tell me the range of variation.
Regards
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The numerical value does not appear in the Electrical Characteristics table in Section 7.5. Please tell me the range of variation.
Regards
Hi,
Please see the FB voltage variation. Thanks.
Best Regards,
Shipeng
Hi Shipeng san
0.763 typ varys from 751 to 799?
or from 0.751*0.763/0.765 to 0.779*0.763/0.765 ?
or from 0.751 + (0.763-0.765) to 0.779 + (0.763-0.765) ?
Is 0.0017 constant?
Hi Hiroshi,
The typical value is 0.765 but there's a drift when Vout>2.5V. But the range is always in 0.751~0.779.
Thanks.
Best Regards,
Shipeng