Part Number: UCC5320
我通过UCC5320来产生-10/25V电压来驱动我的MOS管,同时我需要一个开关来控制驱动IC输出到MOS管的通断。我想知道是否有符合我需求的开关?或者说可以通过更换栅极驱动IC来实现我的需求。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi ??,
You need a gate driver and also a series switch between the gate driver and the MOSFET? What is the required purpose for this second switch?
You can use the UCC5320 to drive a MOSFET directly.
Best regards,
Sean
Our expert will answer the question, but it will help if you could post the question in English if possible.
It sounds like you need a tri-state buffer. There is not a gate driver in our portfolio designed for this purpose. The split output UCC5320S does have two outputs that operate in open drain configuration. Maybe this is useful. Your current implementation is likely a good option.