This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Stas,
My understanding is that you configure the A0, A1, A2 LED in auto mode but only the A0 and A2 are working? Am I correct?
BR, Jared
Yes correct,
And if I enable the A1(Res) and read the status registers of AEU the leds I see value that indicates Error, and none of the leds works.
Hi Stas,
Do you have the EVM of LP5812? Could you please try your configuration on EVM first?
It's because based on your description, I haven't found anything wrong. And I think it's not going to work in theory, because if A0, A2 is fine, A1 must be fine. So, please help to verify your configuration on EVM first. Thanks!
BR, Jared
I use your drivers adopted to my MCU.
I use 0x14 (5bit address). Not broadcast.
In manual mode everything (every led) works fine (as it supposed to work).
I am having troubles only in auto mode.
I also set up registers in your GUI - looks the same I send to the device.
My question mostly: do I setup correct?
May it be some internal LP5812 problems?
What can cause an error? From my understanding error may come only if led is not connected.
Stas
Hi Stas,
You are right!
From my side, I didn't find anything wrong from your configuration. But I don't think it's LP5812 IC problems.
And the format of chip address I mean is just like below:
BR, Jared
I don't have EVM, maybe we should bye one, no problem. I just don't see how it could help. If on EVM with the same setup it will work what it tells me? I2C problems? So why it works in manual mode?
I would be more happy if you tell me I am wrong in setup =)
I want to repeat my question, if possible tell me: what is cause of getting error?
Hi Stas,
I am sorry that I am not sure what's the problem here so far. Please request a EVM and do the same configuration on it. Then, I can tell what's the problem.
BR, Jared
Hi Stas,
Looking forward to your reply!
If you have any result, please free to contact me via email (jared-zhou@ti.com)
BR, Jared
Now we have Passover and work no full power, after holidays we need to discuss with guys our plan.
It is not normal practice that we spent 2 weeks for LED driver and it is still not operational. Maybe we will stay with manual mode because it works, or maybe we will try to get evaluation and achieve autonomous mode.
Thanks for your time and help!
Stas
Hi Stas,
I'm sorry I didn't help, but if you have any time later and want to figure it out. Please free to contact me via email (jared-zhou@ti.com).
BR, Jared
Hi Jared!
We found out problem in I2C driver. Now everything is working.
Thanks.