Hello,
I am working with the bq78pl116 and am experiencing issues with RSOC dropping to zero immediately at the beginning of a discharge.
With a fresh set of cells I connected to the bq78pl116 via BQWizard without any issues. I setup the TMAP file for 4 series cells and select chem type 100. I then calibrated the temp and current successfully. I then setup the various charge and pack parameters within BQWizard. I then issue the Learn/Reinit command within BQWizard and commence charging the pack at 0.2C. With polling turned on I can see the pack charging and the RSOC increasing as expected. The Fully Charged bit is set, pack passed current is approx. 10Ah and RSOC indicated 100%. All seems good. I let the pack rest for at least 2 hours to allow the pack to get into relaxation mode and update. I then start a discharge at 0.5C and the RSOC immediately drops to zero. If i stop the discharge and issue the Learn/Reinit command and restart the discharge the RSOC jumps back up to 100% and updates normally during the discharge period. I have been through several charge/discharge cycles with identical behaviour.
Any help would be greatly appreciated.
Thanks very much,
Patrick