This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS565208: TPS565208 application question

Part Number: TPS565208


Hi team,

some question during design need your help to confirm:

1.When VOUT=0.9V, the datasheet recommend to put the inductor value to be 1uH~4.7uH. is it acceptable to use 1uH? will there be stability risk cause the 1uH is the min value recommended.

2. In some extreme use case, customer may need 6A current for load, TPS565208's OC point is 6.5A, will that means the device can support current up to 6.5A? or it only means it can stand a short time period current up to 6.5A?