Other Parts Discussed in Thread: LM5156, LM51561
Hello All
I am developing isolated DC to DC For as per below specs.
Input - 17 VDC to 32V DC.
Output - 5 VDC
Load - 3A.
Overload current - 3.5A
using which pin of the IC Can I tune Overload current protection?
Please explain working for the same.
Regards
Aditya Yedur