This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25730: PTM mode config

Part Number: BQ25730
Other Parts Discussed in Thread: BQ25713,

We used BQ25713 before, but because we need to increase the voltage in PTM mode to 24V, we considered using BQ25730, but in the actual test, we found that the two chips seem to be a little different in PTM mode, and can not be directly replaced. We only need to configure an EN PTM mode in the manual of BQ25730, and we did so, but in fact the output voltage will drop to 4V. After checking, we found HIDRV1 & HIDRIV2 did not have output, that means Q1 and Q4 did not open.

Therefore, I would like to know how to configure the PTM of BQ25730. Thanks!