This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

3ph 415VAC, 50Hz input to 250V Battery charger , 4kW output

Part Number: no
Other Parts Discussed in Thread: TIDA-01606, PMP21999

Input :3ph input 415VAC, 50Hz,

Output: 230-255 VDC variable

Application: Battery charger, 4kW output.

EMi/ EMC: MIL-STD-461F

Temp: -30 to +55 C

please suggest us Any reference design suitable for above specifications?