hello,
In the bq79631-q1 chip, I sent a low level (wake up sequence) for 2.3ms in the TX pin of the MCU, increased the measured current by 12mA, Both AVDD and DVDD jump to high level , and then sent 1Mbps 8-N-1 [80,00,05,01, F5,8F] data frame using the serial port debugger. However, the Tx of bq79631-q1 has no data and is often high.
It is worth noting that I found that the NFAULT pin was pulled down within 5-10ms of awakening. Do you mean to report a malfunction? This failure will not terminate normal communication.After reset (MCU-TX pulls down 36ms), the NFAULT pin becomes high.
The normal process is not able to communicate normally after sending a wake up sequence.
Looking forward to your reply!
Thanks