Hello
Please, I am having an issue with my gate drive output where one signal looks higher than the other.
Here is the trace:
The green is high-side gate drive with +10/-10V.
Blue is low-side gate drive with +20/-5V.
My problem here is that the green gate drive has a very low Vgs. I would like to know why I am seeing this and what the cause of it is.
I was expecting the same voltage as the blue trace. I have measured the power supply for VDD and VEE. The VDD is showing me +19.4V and VEE -6.51V (green trace), and the blue VDD is +20.5V and -5.1V.
I need some help here, please.
I am using a differential probe with x10 on my measurement.
Regards,
Ikenna.