This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPSM63610: Regarding equivalent IC replacement with higher current rating for TPSM63610

Part Number: TPSM63610
Other Parts Discussed in Thread: TPSM64406

Hello there, 

I need to drive a load of 32A using TPSM63610 IC. In order to use this IC in the design, I need to quadruple the IC for the load requirement since single IC is capable of only 8A max. Can you please suggest any equivalent alternative IC with similar specifications and functionality but with higher current rating.

Thanks,

Sahil Singh