Hi,
According to page 15 of the data sheet, a 10 pF cap in parallel with R3 (FB resistor) is a good workaround for using ceramic caps. I wanted to find out if this is a known good fix.
My layout has 2 TDK C3225X5R0J107M caps. One right next to the TPS61030 and the other exactly on the other side. The via holes are between the cap and the VOUT pins. The ground is connected via a copper flood to the big pad under the TPS61030, and with vias, of course, for the cap on the opposite PCB side from the chip.
I did look at the TPS63020 as one forum posting had suggested, but I think the 61030 is a better fit overall.
I am using the TPS61030 with system 3.3V in and 5V@ 2A out.
I was going to use the TPS61032 but the data sheet recommends TPS61030 if I use ceramic output caps.
Comments?
Thanks!!