Part Number: UCC28180
Hi
I am designing a 2.5KW PFC with ucc28180.
Vinmin=160
Vinmax= 270
Efficiency expected= 98
Vout= 400V
Based on a 40 percent ripple ( Inductor current) I calculated the boost inductor is 156uH.
I have the following questions
1) Whether it is a DC bias inductance or is it a full load inductance??\
2) I have a bigger inductor which is used in another design of 600uH ( bigger core) can carry 25A . What happens if I use this inductor??
3) basically what happens if I use much bigger inductor than calculated one??