Hi Team,
How to test the OCP (Over current protection) function?
I saw that ISW = 2.2~2.65A, so the ISW we measure is PIN1 of the IC or Iin of T1?
Is the test method to increase the current at the output terminal of LM25183?
When the ISW reaches 2.2~2.65A, it will be protected or OCP is activated?
When Iout=0.37A, Iin & Isw both have only about 500mA current. (The red box in the circuit diagram below),
It is different from Isw = 2.2~2.65A marked on the datasheet. What is the reason? Or is the test method wrong?