This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS1211-Q1: Replacement for relay+relay driver with a high side switch

Part Number: TPS1211-Q1
Other Parts Discussed in Thread: TPS1200-Q1

In my board design, I'm trying to replace a Relay + Relay driver configuration, with a single High Side Switch. I need 11 channels with each channel supporting up to 30A.
The specification of the relay used is: Contact Resistance = 4.4mOhm, 30A, Max Switching Voltage =16VDC.
The link to relay data sheet is : www.mouser.com/.../relay_ex1_ex2_e-3315796.pdf

The most idealistic solution I'm looking for is a single Smart High Side Switch, Automotive qualified, with 11 Channels. each channel supports load current of 30A. Please let me know of a solution which is the closest to the above mentioned and can be implemented with minimum cost. the price target per piece of the IC id expected to be < $12.
Thank you