Hi All!
Please take a look at my particular problem with weird behaviour of my circuit.
I have a 6 cell Li-ion package. My target charging voltage is set to 24.66V (with VFB pin), fast charge current set to 1.06A (with ISET1) and termination current to 0.15A (with ISET2).
After plugging the battery all seems fine: STAT1 is OFF (high), PG is OFF (high). After connecting my power source (26VDC, but after schottky diode charger really sees ~25.5VDC) still everything is as expected: PG goes ON (low), STAT1 goes ON (low), STAT2 goes OFF (high) - charger reports that it is indeed charging. I can see it in measured current (~100mA flowing INTO the cells).
Now what is wrong: I disconnect the power source and charger still reports charging - STAT1 stays ON (low), PG stays ON (low)! Basically BQ chip is charging my battery with it's own energy. Why it did not notice that power adapter was disconnected? Simple - because on VCC pin it still sees voltage higher that on SRN ( 23.8V vs 23.0V). Where did this higher voltage came from? It seems that a DC-DC boost converter suddenly emerged, consisting of 2 mosfets and a inductor. And it is BQ chip that drives them (checked on HIDRV and LODRV pins).
Charger seems to be stuck (latched) in this state. I can manually restore 'not charging' state by eg. applying significant load to output, or by shorting out thermistor, and hopefully by shorting CE to GND.
Clearly I missed something fundamental here. Let me show you my schematics:
Please help me understand why this is occuring. Or at least give some hint how to patch this problem. This is 2nd prototype of this board, well into the project and I somehow didn't notice this weird behaviour before. Is BQ24610 even suitable for my product? I'm starting to pull my hair...
Cheers!
Mateusz