This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM7480-Q1: LM7480-Q1: Reason for bidirectional vs unidirectional TVS diode on the input side

Part Number: LM7480-Q1
Other Parts Discussed in Thread: TPS73801

Hello TI,

I was looking at this thread LM7480-Q1: Reason for bidirectional vs unidirectional TVS diode on the input side - Power management forum - Power management - TI E2E support forums regarding usage of uni directional diode where both negative and positive transients are expected.

I am looking for an LDO which can withstand both positive and negative transients at its output pin.  Usually lot of TI LDOs specifies higher voltages on positive side and diode drop on negative voltage typically -0.3V as absolute maximum ratings. So what will happen if i use a unidirectional TVS diode instead of bidirectional TVS on the output ? since it will clamp to higher voltage (lets say +30V) during positive transients and it acts as forward diode for negative transients. will this work for me ? did i miss something ?

Best Regards,

Manoj.