Part Number: TPS7A94
Other Parts Discussed in Thread: TPS7A14, TPS7A53B
Hi, I have a board I'm working on that requires the following power rails:
19V @ 2A
5V @ 3A
3V3 @ 1A
1V05 @ 1A
I'm trying to figure out whether I should be using 4 discrete regulators or a PMIC solution. At which point is it worth it to switch to a PMIC? I'm initially looking at the PMIC option because board space is a little tight, but I would rather not burden the SW team with additional work if I can avoid it. Is a PMIC worth it for this kind of situation, and could anyone recommend one to me that doesn't require much (or hopefully any) SW set up?
Thanks,
Matt